Amphenol Sine Systems is a Global Leader in providing you with interconnection options and solutions. We fulfill your Interconnect Requirements, freeing you up to focus on your core business. More...
BNS Solutions, the design of embedded controls and battery systems are a daily event. BNS Solutions has developed in-house expertise and an extended network to help meet the design needs of our customers. More...
Cymbet is the leader in thin film battery technology and energy harvesting power management solutions. The Cymbet EnerChip™ family of solid-state, rechargeable thin-film batteries is a new innovation in energy management and energy storage. Packaged as a Surface Mount Technology (SMT) component, the EnerChip provides energy storage in a form factor and with a convenience not previously attainable using conventional solutions such as lithium coin cells and super capacitors. Cymbet continues to be a proactive force in the development of green technology thanks to their energy harvesting solutions. More...
Enhanced Video Devices, Inc. provides high-performance video enhancement products based upon its innovative ultra-large kernel processor and core technologies. EVD’s products are designed from the ground up to provide market differentiation, simple integration, and ease of customization in a wide variety of applications, such as consumer, medical, military and security. More...
Fujitsu Microelectronics America, Inc. leads the industry in innovation. FMA provides high-quality, reliable semiconductor products, design and manufacturing services for the wireless, consumer, automotive, and other markets throughout North and South America. More...
mec switches, with a commitment to excellence extending over more than 70 years, facilitates the design and manufacturing of world-class switches and navigators to withstand at least 10 million operations. Sealed to meet IP67 specifications, these mec switches are suitable for multiple applications in a variety of industry sectors including audio/video, broadcasting, instrumentation, medical and defense. When customers require performance, reliability and outstanding design they turn to mec. More...
Rose+Bopla Enclosures manufactures an extensive line of watertight enclosures in Aluminum (cast and extruded), Fiberglass, Polyamide, Polycarbonate, ABS, and Stainless Steel. These durable enclosures are ideally suited for industrial and electronic applications such as instrumentation housings, modular tabletop, machine control, and hand-held enclosures. Protection ratings up to NEMA 4X, IP66, as well as increased safety, an example would be enclosures with ATEX and IECEX certification. More...
Sagrad, Inc. designs and produces a variety of wireless products which include technologies such as 802.11 WiFi modules, phased arrays, frequency converters, UMTS RF systems, GSM, FM audio products and power amplifiers. Sagrad provides both standard products and engineering services to assist customers in rapidly developing products. In addition Sagrad’s Asian company can insure high volume production and world wide competitive prices. Sagrad incorporated in 2004 with headquarters located in Melbourne, Florida. More...
Skyworks Solutions, Inc. is an innovator of high reliability analog and mixed signal semiconductors. Leveraging core technologies, Skyworks offers diverse standard and custom linear products supporting automotive, broadband, cellular infrastructure, energy management, industrial, medical, military and mobile handset applications. More...
Spectra Symbol created the breakthrough form-factor of Membrane Sensor Technology, with 0.5mm height, and has revolutionized how OEMs can use full-travel position feedback. These inexpensive full-travel sensors range from 12.5mm to 1,000mm in stock. For more information, visit www.spectrasymbol.com. Included in the Spectra Symbol product line are the Flex Sensor, medical-grade SoftPot, narrow ThinPot, high temp. HotPot and contactless MagnetoPot Sensors. More...
XMOS is the leader in event-driven processors™ for digital electronics. XMOS event-driven processors™ are high performance, predictable, processors. They allow complete systems to be implemented in software using interface, DSP and control code. More...
View Our Complete Digi-Key Supplier Index