High-Efficiency, Low-EMI, Class D Audio Amps for Portable
Applications
ADI’s Class D amplifier series uses a new tri-level PDM (Pulse Density Modulation) Sigma-Delta architecture to increase overall power efficiency, minimize EMI, and significantly reduce the design effort of utilizing Class D amps in portable applications. This low-noise architecture eliminates the need for external LC output filters. The SSM23xx family of Class D amplifiers has the performance, features, and functionality to significantly simplify system design and deliver the highest quality of audio to the consumer.
- Product Highlights
- Product Training Modules
- Product Listing
- Analog Devices, Inc.
- Archives
SSM2306: This high efficiency, Class-D stereo audio amplifier is designed to maximize performance for portable stereo amplifier applications and is capable of delivering 2 W of continuous output power with less than 1% THD+N, driving a 4-Ω load from a 5.0-V supply. The SSM2306 has a micro-power shutdown mode with a typical shutdown current of 20 nA. The fully differential input of the SSM2306 provides excellent rejection of common-mode noise on the input. It has built-in thermal shutdown and output short-circuit protection and is available in a 16-lead, 3 mm × 3 mm lead frame chip scale package (LFCSP).
SSM2304: The SSM2304 Class-D stereo audio amplifier features a high efficiency, low noise modulation scheme designed to maximize performance of portable applications. It operates with 85% efficiency at 1.4 W into 8 Ω from a 5.0 V supply and has a signal-to-noise ratio (SNR) that is better than 98 dB. Also, PDM modulation is used to provide lower EMI-radiated emissions compared with other Class-D architectures. Additionally, the architecture of the device allows it to achieve a very low level of pop and click minimizing voltage glitches at the output during turn-on and turn-off, thus reducing audible noise on activation and deactivation.
SSM2302: The SSM2302 is a fully integrated, high efficiency, Class-D stereo audio amplifier designed to maximize performance for mobile phone applications. The fully differential input provides excellent rejection of common-mode noise on the input and the architecture of the device allows it to achieve a very low level of pop and click. The typical application circuit requires a minimum of external components and operates from a single 2.5 V to 5.0 V supply. It is capable of delivering 1.4 W of continuous output power with less than 1% THD + N driving an 8 Ω load from a 5.0 V supply.
SSM2301: This fully integrated, high efficiency, Class-D audio amplifier is designed to maximize performance for mobile phone applications. The typical application circuit requires a minimum of external components and operates from a single 2.5 V to 5.0 V supply. It is capable of delivering 1.4 W of continuous output power with less than 1% THD + N driving an 8 Ω load from a 5.0 V supply with an 85% efficiency.
Digi-Key Product Training Modules® are now available. As a continuation of our long-standing commitment to servicing all of our customers' needs from Prototype to Production, Digi-Key, in cooperation with several of our supplier partners, has launched Digi-Key Product Training Modules®. This web-based learning tool, developed by Digi-Key and hosted on www.digikey.com, provides yet another tool for the Engineer's toolbox. This tool facilitates even faster time to market as an Engineer can now learn about the latest products and technologies available, contact Digi-Key technical support, download datasheets, check inventory and place an order for same-day shipping, all from within one Web site. With the addition of this service, Digi-Key has truly become the one-stop shop for all of our customers' needs.
*To view modules, you will need Macromedia Flash 6 software, or greater, installed on your computer. Macromedia/Adobe Flash Player is available FREE from Adobe. Flash Player | Flash Player Support Center

Analog Devices, Inc. (NYSE: ADI) is a world-leading semiconductor company specializing in high-performance analog, mixed-signal and digital signal processing (DSP) integrated circuits (ICs). Since ADI was founded in 1965, its focus has been to solve the engineering challenges associated with signal processing in electronic equipment. ADI's products play a fundamental role in converting real-world phenomena such as temperature, motion, pressure, light and sound into electrical signals to be used in a wide array of applications ranging from industrial process control, factory automation, radar systems and CAT scanners to cellular base stations, broadband modems, wireless telephones, computers, cars and digital cameras.
ADI's unique value to its customers is its ability to overcome the seemingly insurmountable barriers of speed, accuracy and cost, to solve intricate engineering challenges and to create ICs—whether they are general purpose or customized individual components—that enable portability, connectivity and multimedia. ADI designs, manufactures and markets high-performance, high-precision signal processing ICs that make pictures vibrant, voices clear, connections continuous and products portable.
The ADI company brand is recognized throughout the electronics industry for innovative, high-performance technology and world-class engineering support. ADI's portfolio of more than 10,000 products serves the needs of more than 60,000 customers worldwide. ADI's brand, portfolio of products, breadth of customers and core competency in signal processing technology combine to form one of the strongest franchises in the entire semiconductor industry.
ADI currently has a worldwide workforce of approximately 8,600 employees, including 3,100 engineers. There are wafer fabrication facilities using high-performance analog manufacturing processes in Massachusetts, California and Ireland. Additional manufacturing facilities are located in the United States and the United Kingdom. Product test and assembly is conducted at our facilities in the Philippines. Corporate headquarters is located in Norwood, MA, USA.
New Product Highlights
ADI's New High Performance Analog Components
- "Currents" is a quarterly publication (available online and in print) of new products. Get your first look at ADI's New High Performance Analog Components.
Solutions Bulletins Publication Series
- For the latest information on Analog Devices products and design solutions, delve into their Solutions Bulletins publication series. Choose just the product category you are most interested in, or take a full signal chain approach and read them all. Each issue is packed with our newest offerings, design ideas, selection guides, and info on obtaining free samples.
ADI Design Center
Webinar (Archived)
Analog Devices Low Noise Amplifiers available from Digi-Key
Designing a system to meet very low noise requirements can be very challenging. To ensure system noise remains within the overall noise budget, it is crucial to reduce the preamp noise which is propagated and further amplified as the signal progresses through the system. Additionally, reducing preamp noise increases signal-to-noise ratios and allows the conditioning of very low level signals for better signal integrity.
Digi-Key offers a broad range of low noise amplifiers from Analog Devices that will aid in meeting the challenges of the latest design requirements. Choose from the wide variety of high-speed, precision, differential, instrumentation, and variable gain amplifiers to meet any system specification.

|
|
|
|