Digi-Key Stocks C&K ELUM Series SwitchesPushbutton switches designed to eliminate the need for separate LED and light pipe on a printed circuit boardTHIEF RIVER FALLS, Minnesota - May 06, 2009 — Electronic components distributor Digi-Key Corporation, recognized by design engineers as having the industry's broadest selection of electronic components available for immediate shipment, announced today it is now stocking C&K Components' ELUM series switches. Designed to eliminate the need for separate LEDs and light pipes on printed circuit boards, these switches are available on Digi-Key's global websites and are featured in its print and online catalogs. The ELUM Series switches feature a 6mm profile and are available in through-hole and surface-mount configurations. The ELUM features silver- or gold-plated contacts that range in ratings from 0.01mA to 250mA and from 20mV to 50VDC. The latching version (push-push) can be specified for switching functions such as mode select and power on/off, while the momentary version is ideal for test, reset and notification functions. The ELUM Series device is one of the only pushbutton switches designed so the LED travels with the actuator, ensuring even distribution of light. The compact design saves space on the PC board, enabling product miniaturization and greater on-board functionality. ELUM Series switches are RoHS-compliant and compatible with high-speed reflow soldering processes. The 30,000-cycle life expectancy makes the pushbutton devices ideal for telecom, industrial, medical, automotive, and consumer electronics applications. To learn more about this product, view the "ELUM™ Illuminated Pushbuttons" PTM Online... On Demand® product training module on Digi-Key's websites. This new training module introduces the product as well as discussion of physical and electrical options and applications for these switches. About Digi-Key CorporationOne of the world's fastest growing distributors of electronic components, Digi-Key has earned its reputation as an industry leader through its total commitment to service and performance. As a full-service provider of both prototype/design and production quantities of electronic components, Digi-Key has been ranked #1 for Overall Performance for 17 consecutive years from among the nation's more than 200 distributors (EE Times Distribution Study/August 2008). Offering more than 1.5 million products from nearly 400 quality name-brand manufacturers, Digi-Key's commitment to inventory is unparalleled. Access to the company's broad product offering is available 24/7 at Digi-Key's top-rated website, www.digikey.com. About C&K ComponentsC&K Components leads the industry in the design and manufacturing of detect, DIP, navigation, pushbutton, rocker, rotary, slide, snap, switchlock, tactile and toggle switches as well as smart card interconnect devices and high reliability connectors. C&K offers more than 40,000 unique part numbers that are built, priced and delivered as standard catalog items. C&K has state-of-the-art design centers in Europe, North America and Asia, which include complete in-house testing facilities in each region. C&K offers flexible manufacturing capable of scaling production from prototype design through volume production and also offers a wide range of value-added solutions, from wire leads and harnesses to complete front panel assemblies. For more information about C&K Components, visit www.ck-components.com.
|